NX About [Include Subassemblies] option for Parts List command.

2021-12-15T06:27:22Z
NX for Design

Summary


Details

About [Include Subassemblies] option for Parts List command.

Solution

From the Parts List.
You need to be select the "Select Object" option when selecting the "Include subassembly" option.

Includes or excludes the components of a subassembly when it is selected from the Assembly Navigator or from the graphics window.

When "Include subassembly"; OFF
The only subassembly is added in the Parts List. Refer below Image-1

Image-1

When "Include Subassembly"; ON
The subassembly, as well as included components in subassemblies, are added in the Parts List. Refer below Image-2

Image-2.


Notes and References

10221505

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1953
Function: TABLES

Ref: 002-8600556

KB Article ID# PL8600556

Contents

SummaryDetails

Associated Components

Drafting